Programming STM32H745i with St-link v2
When programming STM32H745i with St-link v2 I notice that the display does not turn on, only LD2 flashes red and can not load the code giving the following message:
stmcubeide v1.16.0 upgraded stlink v2 without problems and recognizes it well.

In the schematic I did not seem to see any jumper that has to do with the power supply of the st-link.
Did I miss to do something besides connecting (SWDIO,GND,SWCLK,3.3V)?
I even tried to power it by USB and connect the st-link v2 without the 3.3V but it didn't work either.