Question
Programming the board using a USB connection. (at Nucleo-G491RE)
- December 16, 2025
- 4 replies
- 96 views
Hello,
First, I would like to express my deepest gratitude for your assistance.
I intend to update the firmware using STM32CubeProgrammer with the following hardware configuration

Additionally, I have set the Boot0 pin to High using a jumper.
However, my PC is not detecting DFU mode.
Additionally, the programmer is not recognizing the USB connection.


Did I miss anything?
PS. The board has undergone a full chip erase.