Question about interfacing 4 I2S microphones with STM32F4
Hi I am designing a PCB for sampling 4 audio channels from 4 I2S MEMs microphone and doing some audio processing on it. My MCU STM32F407 has 5 I2S peripherals and I plan to use I2S2 and I2S3 for each pair of microphones. The configuration of each I2S is below (same for both):


My question is let's say I start I2S2 and I2S3 like following:
// 4000 samples (24 bits over 32-bit word)
uint32_t * first_buffer = malloc(4000 * sizeof(uint32_t));
uint32_t * second_buffer = malloc(4000 * sizeof(uint32_t));
// DMA transfer size is byte, hence * 4
HAL_I2S_Receive_DMA(&hi2s2, (uint16_t *) first_buffer, 4000 * 4);
HAL_I2S_Receive_DMA(&hi2s3, (uint16_t *) second_buffer, 4000 * 4);Would there be a delay between the two microphone pairs? Like I2S2 starts first so first element in first_buffer is actually sampled before first element in second_buffer?
If so, is there any way to synchronise between the two I2S?
Thanks