Questions regarding Audio LE Compatibility with the module
I would like to ask your team some of questions regarding the STM32 module kit which comes with BLE- 5.3 or BLE5.4, I want to make a device which works on BLE-5.3 or 5.4. I want to establish an AudioLE call by using your microcontrollers, Can I use AudioLE with any STM controller, If yes then how can I and if not then shall I do to make it work?
Will it work on full-duplex or half-duplex communication?
Can a 2 ways communication be possible using a single STM or will I need 2 STM to have a communication? Or can I use multiple channels with a single STM for communication?
Please answer these questions I have as soon as possible.
Thanks