Recommendations for VCAP1 on LQFP64 packages
Hello,
I've been looking into using a STM32F722RET6, which comes in the LQFP64 package. This package only has one VCAP pin, and the datasheet states that the capacitor on this pin should have a capacitance of 4.7 uF, and an equivalent series resistance between 0.1 and 0.2 ohms. It seems as though this is the case for any package that lacks the VCAP2 pin. If anyone has had success using one of these packages, would you be able to recommend a capacitor for this application? It seems very few of the ceramic capacitors on DigiKey list their ESR.