Request review schematics & PCB using STM32F401VET6(expecially ESD)
Dear STMicroelectronics,
The attached file is a product circuit diagram applying STM32F401VET6 as the main CPU.
As for the inquiry, there is a problem that the CPU standard output HIGH signal drops to LOW signal at a specific PORT when performing ESD test.
The specific PORT is as follows.
=>PB2,PB3,PB4,PB5,PB6,PB7,PB8,PB9,PB10,PB12,PB13,PB14,PB15,PC0,PC1,PC2,PC3,PC4,PC5,PC6,PC8,PC9,PC10,PC11. PC12, PC13
=> A specific PORT is the input signal (Base) of the PNP Transitor-applied switching circuit, and functions to turn on (High) and turn off (Low) the LED.
Please review the attached circuit diagram and PCB.
Thank you.