Resistor values for Vbus sensing
Goodmorning,
I am using STM32L552RCT6 in my design that I intend to use through a USB interface.
I'm trying to implement the VBUS sense (compulsory since my device will be self-powered). I have read AN4879, and it's clear to me that I have to add a voltage divider to avoid the situation where I provide 5V to the MCU while it's not powered. The values recommend from AN4879 makes perfect sense too.

However, I checked the schematics of the NUCLEO-L55ZE-Q, and the values of the resistor there are very much different!

Can anyone explain to me why there is this discrepancy and which one I should follow?
Thanks!