[RESOLVED] VCP on ST-LINK v3 mini
I cannot get the VCP function of ST-LINK v3 mini working.
Windows sees the com port and can open it
Connected TX output of UART to pin 14 of ST-LINK 3 mini, but nothing is received on the PC side.
Connected some other serial TTL-USB adapter (set to 3.3V), and it works properly.
However, the serial TTL-USB adapter has a ground connection and ST-LINK's VCP has common ground with other functions.
The debugger function works properly.
Is the TX level of VCP 3.3 or 5 V? Does the VCP function work for anyone?
Thanks,
-- pa