Riverdi_101 STM32H7: ST-Link can't connect to board
For more than 3 days I am trying to solve a problem of connecting to Riverdi board using external ST-link from a discovery board. I flashed apps without problem and now I can't do anything. I remember last time I was flashing an app it asked that firmware of St-link has to be updated before continuing so I proceeded. I successfully flashed the app but now I am unable to flash it again.
13:07:23 : STM32CubeProgrammer API v2.18.0 | Windows-64Bits
13:07:27 : UR connection mode is defined with the HWrst reset mode
13:07:27 : ST-LINK SN : 0670FF3332584B3043153854
13:07:27 : ST-LINK FW : V2J45M31
13:07:27 : Board : STM32F4DISCOVERY
13:07:27 : Voltage : 2.91V
13:07:27 : Error: Unable to get core ID
13:07:27 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
If I try to connect to other boards It is connected without problem.
Please help,
Regards