Question
RJ45 & Ethernet in NUCLEO-U575ZI-Q
Hi,
I have seen on the website that the NUCLEO-U575ZI-Q board includes Ethernet RJ45 (under the Moard-specific features): https://www.st.com/en/evaluation-tools/nucleo-u575zi-q.html
However, it doesn´t appear in the user manual (UM2861) and I can´t find the connector on the pictures, Is that a mistake or am I missing something? Thanks!
- Board-specific features
- External or internal SMPS to generate Vcore logic supply
- Ethernet compliant with IEEE-802.3-2002
- USB OTG full speed or SNK/UFP (full-speed or high-speed mode), depending on the USB connector type
- Board connectors:
- USB with Micro-AB or USB Type-C®
- Ethernet RJ45