Robotdyn STM32 Black Pill not recognised when connected to ST-Link v2 (SOLVED)
I have 4 STM32 boards. Two very cheap Blue Pill boards (from two different suppliers), and two RobotDyn Black Pill boards (from another two completely different suppliers). I also have two ST-Link v2 clone type USB adapters - one with the original firmware that it shipped with (V2.J24.S4) and one that was updated to the latest ST firmware (V2.J33.S7) using the ST Utility. When I plug either of my Blue Pill boards into either of the ST-Links, the ST Utility can "see" them and I can use my Arduino IDE to program them. However, when I plug either of my RobotDyn Black Pill boards into either one of the ST-Link adapters, neither the ST-Link Utility nor the Arduino IDE can recognise them. the ST-Link Utility says that it cannot connect to target and the Arduino IDE says "No target connected". I'm sure that I'm missing something silly or blindingly obvious here, but I just can't work out what. The Robotdyn boards are supposed to be far better built than the standard Blue Pill boards, but it's the Black Pill boards that I can't get working, & the Blue Pill boards worked straight away. What am I doing wrong please?