Skip to main content
Visitor II
November 21, 2025
Question

RTC precision on H573I-DK board

  • November 21, 2025
  • 3 replies
  • 163 views

Hi,

I'm running test on the Discovery board H573I-DK.

On a 24 hours period, I measure a 340 ppm precision that is far from the 20 ppm of the LSE Quartz.

Is it normal ?

    This topic has been closed for replies.

    3 replies

    Graduate II
    November 21, 2025

    Did the board run to slow? If  yes, was the board running continious or did resets happen as caused by loading a new programm. It is quit easy to stop the RTC for some short period during programm startup  while the startup code checks the status of the RTC.

    Technical Moderator
    November 21, 2025

    Hello @emd64 and welcome to the community,

    Refer also to this knowledge base: How to calibrate the STM32's real-time clock (RTC)

    Super User
    November 21, 2025

    > I'm running test

    What test?

    > I measure a 340 ppm precision

    How do you measure that?

    Read out and check/post content of RCC_BDCR and RTC registers.

    Also, as @Uwe Bonnes said above, Cube/HAL used to (and may still do?) cause RTC to be delayed upon each reset.

    JW