Seeing opposite behavior expected from an open drain output?
I am working with the NUCLEO-L552ZE-Q and have made a very simple test circuit to test an open drain output signal. I have the pin configured as an open drain output with no pull up or pull down with the signal pulled up to 3.3V through a 1K resistor. When I SET the pin, I see a 3.3V signal probing on the bottom side of the 1K resistor and when I CLEAR the pin, I see a 0V signal. This is opposite of what I would expect? Is there some inverting buffer that is connected to the gate of the fet?