Setting VTOR for Application at 0x90000000 on STM32H735
Hi ST Community,
I am working on a bootloader for my STM32H735 board, and I'm encountering issues with setting the Vector Table Offset Register (VTOR) correctly for my application, which is loaded at address 0x90000000. The main problem I'm facing is that the Ethernet interrupt is not firing as expected, which leads me to believe that the VTOR might not be correctly set.
Here's a brief overview of my setup:
Bootloader Configuration:
My bootloader is running from the internal flash, and it attempts to jump to the application located at 0x90000000.
/* Bootloader Code */
#define APPLICATION_ADDRESS 0x90000000
typedef void (*pFunction)(void);
pFunction JumpToApplication;
void Bootloader_JumpToApplication(void)
{
/* Disable global interrupts */
__disable_irq();
/* Disable SysTick interrupt */
SysTick->CTRL = 0;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);
/* Set the Vector Table Offset Register to the application address */
SCB->VTOR = APPLICATION_ADDRESS;
/* Get the application's reset handler address and jump to it */
JumpToApplication = (pFunction) (*(__IO uint32_t*) (APPLICATION_ADDRESS + 4));
__enable_irq();
JumpToApplication();
/* We should never get here as execution is now on user application */
while(1) { }
}
2. Main Application Configuration:
In my main application, I also try to set the VTOR to ensure it's correctly pointing to the application's vector table.
int main(void)
{
__disable_irq();
SCB->VTOR = 0x90000000;
__DSB(); // Data Synchronization Barrier
__enable_irq();
SCB_InvalidateICache();
SCB_InvalidateDCache();
MPU_Config();
SCB_EnableICache();
SCB_EnableDCache();
HAL_Init();
SystemClock_Config();
if(Memory_Startup() != MEMORY_OK)
{
Error_Handler();
}
CPU_CACHE_Disable();
// Main application logic
while (1)
{
}
}
3. Linker Script:
My linker script is configured as follows:
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1); /* end of RAM */
_Min_Heap_Size = 0x1000; /* required amount of heap */
_Min_Stack_Size = 0x1000; /* required amount of stack */
MEMORY
{
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
FLASH (rx) : ORIGIN = 0x90000000, LENGTH = 64M
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 320K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 32K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 16K
OCTOSPI (xrw) : ORIGIN = 0x70000000, LENGTH = 16M
}
SECTIONS
{
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/* Other sections follow */
}
Despite this setup, the Ethernet interrupt never triggers, which leads me to suspect an issue with the VTOR configuration.
I have also tried enabling #define USER_VECT_TAB_ADDRESS in the system_stm32h7xx.c file, but unfortunately, this did not resolve the issue.
Has anyone faced a similar issue or could provide insights on what might be going wrong? Any suggestions or advice on properly setting the VTOR or debugging this issue would be greatly appreciated.
Thank you in advance!
Cheers,
Emo