Simple LCD display (ILI9341 drivers) - Nothing works
Hello,
I have NUCLEO-H755 + GFX02Z1. With ST examples (X-CUBE-DISPLAY), nothing works (no QSPI available to select).
So i have no configured memory (QSPI on GFX02Z1 board) , only ILI9341 driver.
The MX_DISPLAY_Init looks OK.
I just want to send something to write to the LCD but nothing happened.
My understanding is that it is not mandatory to have external memory to display, I can use internal STM32 memory. Is it true ?
When we perform a BSP_LCD_WriteData, some is written on FMC_BANK1_MEM (because FMC configured on NOR 1.../LCD1).
But how to send from FMC_BANK1_MEM to LCD ?
MX_FMC_Init(); & MX_DISPLAY_Init(); looks good.
I want to do a BSP_LCD_WriteData(0,(uint8_t*)"Hello to everyone!",400), nothing happened.
I can't use TouchGFX example (https://community.st.com/t5/touchgfx-and-gui-mcu/x-cube-display-example-on-nucleo-u575zi-q-with-x-nucleo-gfx02z1/td-p/80066/page/2) because there is not example for NUCLEO-H755...
Thanks for your answers to help me to display anything on this screen !!!! :)
PS : What is strange is that during BSP_LCD_Init, ILI9341_LCD_Driver.ReadID (ReadID4 of ILI9341 driver) is correct (h009341). After init, when I want to read same ID with same function, return is h414141 ... Can't found why at this moment ....