small form factor STM32 boards ...
Doing a short search, I did not find a board that conveniently fits my criteria for some future projects.
These criteria are the following :
- small form factor (not bigger than a Rasperry Pico, preferably smaller (Seed XIAO);
- MCU preferably ranging from C0, F0...F3, F40x, L0 or L1; (not an exclusive list)
- reasonable commercial availability in Europe;
I intend to use these board as a kind of sensor extension for Linux SBCs, with the Raspberry Pi Zero (II) as favourite. Thus the Pi Zero / Pi Pico format as upper size limit.
I can't specify more IO details yet, but the average peripherals of above mentioned MCU variants suffices for most purposes. But at least 8 or more IO lines should be available. Peak performance and low-power capabilities are not a criterium either.
If someone here knows such a board, I would welcome any suggestion.
Thanks !