[SOLVED] ST-LINK V2 Connection Issue with Custom Boards
Hi,
I designed and tried to use my custom board based on STM32F030R8T6 MCU. But the problem started from beginning.
For MCU Flashing I used STM32CubeProgrammer and ST-LINK V2 (STM8 & STM32) dongle.
First of all I was trying to connect the board and I've got "No STM32 target found!" Error.
Second, after NRST Reset button was pressed (this option I considered on my board) and STM32CubeProgrammer Connect pressing, releasing NRST Reset button I succeeded to connect the MCU.
After that, I've erased the chip completely and tried to flash my bin file. But I've got errors reg., Connection to device is lost.
There are two errors in the log list: "Unable to read device id from ROM table" and "Unable to get core ID".
I thought it was problem with board soldering and used another board. But the same issue was with second board as well.
Is there any solution how to rectify the above problem? Did anybody has such issue on custom boards?
Thanks in advance.