ST-Link and J-Link not work well with STM32F745VEH6
Hi team I have a problem on debugging STM32F745VEH6 with SEGGER J-link and ST-Link V3. And phenomenon is different on both debugger.
My enviroment:
STMCubeIDE Ver.1.8.0
Debbuger: ST-Link V3/V2 and SEGGER J-Link Ultra +
MCU: STM32F745VEH6
With ST-Link V2:
Works fine.
With ST-Link V3:
After download program, go to HardFaul_Handler function and crash.
There is a data mismatch address error when download the code.
With J-Link:
Program can download. But live expression and expression not work.
Variable does not update when write it.
When the debugger is detached, the value is updated.
With ST-Link and STM32CubrProgrammer:
Both version of ST-Link outputs DEV_TARGET_RESET_ERR error.
With J-Link and J-Flash app:
Connection is fine.
What could be the cause? And how can I solve it?