ST-Link Automatic mode issue
Hi, with the latest release of ST-Link 4.5.0 i've a problem using 'Automatic Mode'.
I click 'Start' button, attach the cable to my board, and the flash is done. I detach the cable, change the board, attach the cable to new board, but nothing is done. The software seems don't recognize the new board. In this situation if i disconnect the cable from my pc and reconnect to ST-Link, the software recognize the board and flash the software. Waiting for the device number 3, but here same problem occours, for recognize new board i've to disconnect/connect the cable everytimes.
In this situation 'Automatic Mode' works only for the first board, after the flashing i've to disconnect/connect (practically a reset) the ST-Link for recognize the others board.
Here is the software i used:
ST-Link 4.5.0
ST-LinkUsbDriver 5.1.2
ST-Link-CLI 3.5.0
ST-Link Windows Driver 2.1.0
'Automatic Mode' is very useful for flashing many boards...
What can i do?
Thanks