ST-Link cannot more flash external Target
Hello,
Situation: I have a Nucleo WB55 board that is able to flash the internal SMT32 micro with the embedded ST-Link.
I want to use this Nucleo to flash a custom board with the embbedded ST-LINK, disconnecting the jumpers and connecting the lines properly to the custom board. This process fails because Cube programmer don't find the STM32 target. It finds st-link of course and I tried every mode, every clock frequency, everithing.
So this Nucleo can flash internal target but not external one!
Strange things: With the same Nucleo weeks ago I was able to flash external target, now I can't, something happened.
Connections and continuity is OK, custom board is ok (I can flash it with others Nucleo boards), cables are ok, lines are properly connected.
So what a mistery is this?