Skip to main content
Visitor II
October 24, 2013
Question

ST-link_CLI.exe verify function is not working

  • October 24, 2013
  • 1 reply
  • 634 views
Posted on October 24, 2013 at 10:30

When I run the CLI tool for programming including a verify, this is not working:

R:\Shared\Evertz\Automatic ST-link program>ST-LINK_CLI.exe -P ''SYGDR scripts/Boo

tloaderSTM32F0xx-v02.bin'' -V 0x08000000

STM32 ST-LINK CLI v1.4.0

STM32 ST-LINK Command Line Interface

Connected via SWD.

Device ID:0x440

Device family :STM32F05x

Flash Programming:

  File : SYGDR scripts/BootloaderSTM32F0xx-v02.bin

  Address : 0x00000000

[0x00000000]:Invalid address!

When I only do a program it works fine,

Does anyone has any idea what is going on?

#st-link-cli-verify
    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 24, 2013
    Posted on October 24, 2013 at 12:07

    Hi Evert,

    Try to put the address before the ''-V'' option.

    There is a newer version of ST-LINK CLI (v1.7.0) available with

    http://www.st.com/web/en/catalog/tools/FM147/SC1887/PF258168

    .

    -Mayla-