Skip to main content
Visitor II
October 13, 2021
Question

ST-Link fails due to too high RDP by mistakes. How to initialze to factory defaust if possible.

  • October 13, 2021
  • 1 reply
  • 967 views

I came across a fatal trouble, Connecting ST-Link always fails.

This was caused unexpected RDP operation in the debug, that may have changed RDP=1.

It was observed that 'some' program is always starts even after Reset. In my observation, UART is survived. I have lost any way to update the broken FLASH.....

I would like to know ANY solution, such as 1) how to reset to factory defact, or 2) how to activate internal farmware which can make any recovery and what else.

The Target is STM32U575 ZI (144 pin)

Thanks.

Sumi. Nishie

    This topic has been closed for replies.

    1 reply

    Super User
    October 13, 2021

    STM32CubeProgrammer can be used to change RDP level 1 to RDP level 0. It should be changeable in the option bytes. However, RDP level 1 shouldn't cause the ST-Link connection to fail, so perhaps you have something else going on. Try to connect under reset.