ST-Link server is required error after macOS update
Hello, I have been using the same cubeIDE debugger options for several months and have not had any major issues. However i recently updated to the latest macOS 15.0 release (not necessarily the cause, but it's the only change that comes to mind) and since then i've been getting the following error:

I have reinstalled the stlink server as recommended in:
https://community.st.com/t5/stm32cubeide-mcus/st-link-server-is-required-to-launch-the-debug-session/td-p/69617
and
https://community.st.com/t5/stm32-mcus-boards-and-hardware/cubeide-does-not-see-st-link-server/td-p/149158
This has not fixed it and the stlink-server appears to be installed properly as i can use it via the CLI. I have also tried reinstalling the cubeIDE and used different versions of the cubeIDE.
Has anyone encountered something similar or have any idea on what this could be?
EDIT:
I can also host a server from the CLI and connect to it from the cubeIDE via the "Connect to remote GDB server" option.