ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver signed for Windows7, Windows8, Windows10
Downloaded the subject driver and installed it per the instructions in the readme.txt (ran the batch file as admin)
"Device Driver Installation Wizard" dialog reports that the drivers (Qty 3) were successfully installed and ready to use.

In Windows "Device Manger" > "Other devices" the only entry is a pre-existing one "Bluetooth Peripheral Device"
What do I need to do to get the driver to show up in Device Manager?
Connected the board to the Windows computer using a USB to USB micro cable.
The ST-LINK LED flashes on/off about once per second.