Skip to main content
Visitor II
November 4, 2019
Question

ST-LINK upgrade under Linux fails, do other options exist?

  • November 4, 2019
  • 6 replies
  • 2909 views

There were several issues so I am not certain which is the real issue.

  1. I am using STM32CubeIDE version 1.1.0
    1. Note I believe ST needs to consider more carefully how to install things and give direction when something seems wrong in installation. I believe one issue is that ST installs under linux assuming the user is part of the group SUDO, this is dangerous, the only thing that should be installed with root access are drivers, which were part of the installation. /opt however ended up belonging to root:root and it should have been root:users so other people than root uses it. Just saying "this needs a bit of thinking" for installation under Linux, I suppose windows installs are more complicated.
    2. upgrading from 1.0.2 did not work and required a full reinstallation
  2. the board I am attempting to use is a NUCLEO-L476RG with version
    1. STM32CubeIDE demands an upgrade for the ST-Linux Firmware
      1. Error in final launch sequence:
      2. Error in initializing ST-LINK device.
      3. Reason: (6) ST-LINK firmware upgrade required.
      4. Please upgrade the ST-LINK firmware using the upgrade tool. Reconnect ST-LINK and click OK
      5. Error in initializing ST-LINK device.
      6. Reason: (6) ST-LINK firmware upgrade required.
      7. Please upgrade the ST-LINK firmware using the upgrade tool. Reconnect ST-LINK and click OK
    2. Execute upgrade tool
      1. version 3.3.1
      2. Open Update mode
      3. version V2J31M21, upgrade version V2J34M25
      4. Reports
        1. Upgrade error, Please try again.
        2. Upgrade successful. (it wasn't)

Those are the details. I would like to use the ST-Link utility as is available under windows, but it's NOT available under Linux. Wine will not work because windows drivers for USB won't work under wine. The last time I had this issue I had to use a windows machine to do the upgrade. I prefer to not to have to do that.

I hope someone has thoughts and suggestions to help rectify this, as I can't do anything if the debugger refuses to work without upgrading ST-LINK on the target device.

Thank you for any help ahead of time!

    This topic has been closed for replies.

    6 replies

    Graduate II
    November 5, 2019

    Probably the stsw-link007 is already installed. If not, do so. Locate STLinkUpgrade.jar

    > /opt/spare/bon/stm/stsw-link007-201908/AllPlatforms/STLinkUpgrade.jar

    Change to that directory

    > cd /opt/spare/bon/stm/stsw-link007-201908/AllPlatforms/

    Check that you have access rights to the device. Satisfy all requirements for java.

    > java -jar STLinkUpgrade.jar

    Now you should be able to do the upgrade.

    sphil.931Author
    Visitor II
    November 5, 2019

    0690X00000ArhEWQAZ.png0690X00000ArhElQAJ.png0690X00000ArhF5QAJ.png0690X00000ArhEqQAJ.pngI would hazard to guess a few images to give a better description, in addition I ran a few tests.

    I've given images to show what I am seeing.

    I ran the upgrade JAR as root. With the same results (had to do some work using Xephyr to have any output but that is a digression).

    However additional output from the CLI was available:

    "libusb: error [udev_hotplug_event] ignoring udev action bind

    libusb: error [udev_hotplug_event] ignoring udev action bind"

    was output when attempting to upgrade.

    sphil.931Author
    Visitor II
    November 5, 2019

    PS Thanks Uwe Bonnes,

    I grabbed the stsw-link007 latest and did exactly what you suggested (while you were suggesting it appears).

    Their appears to be a number of STLinkUpgrade.jar files floating around in /opt/st/ directory. Each have a different version from 3.3.0 to 3.3.1 I used 3.3.2 when I directly grabbed the update file from ST.

    Just in case I used these directions to be sure it wasn't the "same old problem":

    http://www.emcu.eu/how-to-update-the-st-link-fw-under-linux/

    My install of STCubeMxIDE 1.1.0 seemed to just write over 1.0.2 directory as nothing was added to the structure despite having 1.1 plugins in the directories.

    Graduate II
    November 6, 2019

    Check for flacky cables or some under-powered USB hub or some other problem on your side. Perhaps try on another PC.

    The different STLinkUpgrade.jar files come with different stlink firmware versions.

    sphil.931Author
    Visitor II
    November 8, 2019

    Right checked cables switched hubs.

    Removed hub and direct connected to computer.

    Same results.

    Then I turned on wireshark and tested updating with these results:

    0.00000 GET DESCRIPTOR Request DEVICE
    0.00192 GET DESCRIPTOR Response DEVICE
    0.00194 GET DESCRIPTOR Request DEVICE QUALIFIER
    0.00592 GET DESCRIPTOR Response
    0.00594 GET DESCRIPTOR Request DEVICE QUALIFIER
    0.00892 GET DESCRIPTOR Response
    0.00893 GET DESCRIPTOR Request DEVICE QUALIFIER
    0.01192 GET DESCRIPTOR Response
    0.01194 GET DESCRIPTOR Request CONFIGURATION
    0.01592 GET DESCRIPTOR Response CONFIGURATION
    0.01593 GET DESCRIPTOR Request CONFIGURATION
    0.01892 GET DESCRIPTOR Response CONFIGURATION
    0.01894 GET DESCRIPTOR Request STRING
    0.02192 GET DESCRIPTOR Response STRING
    0.02193 GET DESCRIPTOR Request STRING
    0.02492 GET DESCRIPTOR Response STRING
    0.02493 GET DESCRIPTOR Request STRING
    0.02792 GET DESCRIPTOR Response STRING
    0.02793 GET DESCRIPTOR Request STRING
    0.03092 GET DESCRIPTOR Response STRING
    0.03115 SET CONFIGURATION Request
    0.08791 SET CONFIGURATION Response
    0.08797 GET DESCRIPTOR Request STRING
    0.09091 GET DESCRIPTOR Response STRING
    0.09109 GET DESCRIPTOR Request STRING
    0.09391 GET DESCRIPTOR Response STRING
    0.09454 GET DESCRIPTOR Request STRING
    0.09691 GET DESCRIPTOR Response STRING
    0.09772 SET LINE CODING Request
    0.09991 URB_CONTROL out
    0.10019 GET DESCRIPTOR Request STRING
    0.10290 GET DESCRIPTOR Response STRING
    0.89591 GET DESCRIPTOR Request STRING
    0.89777 GET DESCRIPTOR Response STRING
    0.89803 URB_BULK out
    0.90076 URB_BULK out
    0.90082 URB_BULK in
    0.90176 URB_BULK in
    1.11601 GET MAX LUN Request
    1.11773 GET MAX LUN Response
    1.12204 SCSI: Inquiry LUN: 0x00 
    1.12372 URB_BULK out
    1.12375 URB_BULK in
    1.12472 SCSI: Data In LUN: 0x00 (Inquiry Response Data) [SCSI transfer limited due to allocation_length too small]
    1.12474 URB_BULK in
    1.12772 SCSI: Response LUN: 0x00 (Inquiry) (Good)
    1.12894 SCSI: Test Unit Ready LUN: 0x00 
    1.13072 URB_BULK out
    1.13187 URB_BULK in
    1.13372 SCSI: Response LUN: 0x00 (Test Unit Ready) (Good)
    1.13379 SCSI: Read Capacity(10) LUN: 0x00 
    1.13472 URB_BULK out
    1.13477 URB_BULK in
    1.13772 SCSI: Data In LUN: 0x00 (Read Capacity(10) Response Data) 
    1.13774 URB_BULK in
    1.14072 SCSI: Response LUN: 0x00 (Read Capacity(10)) (Good)
    1.14206 SCSI: Mode Sense(6) LUN: 0x00 
    1.14372 URB_BULK out
    1.14374 URB_BULK in
    1.14472 SCSI: Data In LUN: 0x00 (Mode Sense(6) Response Data) 
    1.14473 URB_BULK in
    1.14772 SCSI: Response LUN: 0x00 (Mode Sense(6)) (Good)
    1.14779 SCSI: Mode Sense(6) LUN: 0x00 
    1.14872 URB_BULK out
    1.14873 URB_BULK in
    1.15172 SCSI: Data In LUN: 0x00 (Mode Sense(6) Response Data) 
    1.15173 URB_BULK in
    1.15471 SCSI: Response LUN: 0x00 (Mode Sense(6)) (Good)
    1.15496 SCSI: Test Unit Ready LUN: 0x00 
    1.15572 URB_BULK out
    1.15573 URB_BULK in
    1.15871 SCSI: Response LUN: 0x00 (Test Unit Ready) (Good)
    1.15877 SCSI: Prevent/Allow Medium Removal LUN: 0x00 PREVENT
    1.15972 URB_BULK out
    1.15973 URB_BULK in
    1.16271 SCSI: Response LUN: 0x00 (Prevent/Allow Medium Removal) (Check Condition)
    1.16273 SCSI: Request Sense LUN: 0x00 
    1.16371 URB_BULK out
    1.16372 URB_BULK in
    1.16671 SCSI: Data In LUN: 0x00 (Request Sense Response Data) 
    1.16673 URB_BULK in
    1.16971 SCSI: Response LUN: 0x00 (Request Sense) (Good)
    1.16977 SCSI: Test Unit Ready LUN: 0x00 
    1.17071 URB_BULK out
    1.17072 URB_BULK in
    1.17371 SCSI: Response LUN: 0x00 (Test Unit Ready) (Good)
    1.17375 SCSI: Read Capacity(10) LUN: 0x00 
    1.17471 URB_BULK out
    1.17472 URB_BULK in
    1.17771 SCSI: Data In LUN: 0x00 (Read Capacity(10) Response Data) 
    1.17772 URB_BULK in
    1.18071 SCSI: Response LUN: 0x00 (Read Capacity(10)) (Good)
    1.18076 SCSI: Mode Sense(6) LUN: 0x00 
    1.18171 URB_BULK out
    1.18172 URB_BULK in
    1.18471 SCSI: Data In LUN: 0x00 (Mode Sense(6) Response Data) 
    1.18472 URB_BULK in
    1.18771 SCSI: Response LUN: 0x00 (Mode Sense(6)) (Good)
    1.18775 SCSI: Mode Sense(6) LUN: 0x00 
    1.18871 URB_BULK out
    1.18872 URB_BULK in
    1.19171 SCSI: Data In LUN: 0x00 (Mode Sense(6) Response Data) 
    1.19172 URB_BULK in
    1.19471 SCSI: Response LUN: 0x00 (Mode Sense(6)) (Good)
    1.19505 SCSI: Read(10) LUN: 0x00 (LBA: 0x00000000, Len: 8)
    1.19571 URB_BULK out
    1.19572 URB_BULK in
    1.20271 SCSI: Data In LUN: 0x00 (Read(10) Response Data) 
    1.20272 URB_BULK in
    1.20571 SCSI: Response LUN: 0x00 (Read(10)) (Good)
    1.20582 SCSI: Read(10) LUN: 0x00 (LBA: 0x00000008, Len: 8)
    1.20671 URB_BULK out
    1.20672 URB_BULK in
    1.21370 SCSI: Data In LUN: 0x00 (Read(10) Response Data) 
    1.21372 URB_BULK in
    1.21670 SCSI: Response LUN: 0x00 (Read(10)) (Good)
    1.21677 SCSI: Read(10) LUN: 0x00 (LBA: 0x00000018, Len: 8)
    1.21770 URB_BULK out
    1.21772 URB_BULK in
    1.22470 SCSI: Data In LUN: 0x00 (Read(10) Response Data) 
    1.22472 URB_BULK in
    1.22770 SCSI: Response LUN: 0x00 (Read(10)) (Good)
    1.22806 SCSI: Test Unit Ready LUN: 0x00 
    1.22870 URB_BULK out
    1.22873 URB_BULK in
    1.23170 SCSI: Response LUN: 0x00 (Test Unit Ready) (Good)
    1.23175 SCSI: Test Unit Ready LUN: 0x00 

    sphil.931Author
    Visitor II
    November 8, 2019

    It looks like it recognizes it as a st-link and then sets it up has a USB mass storage device.

    What the Heck?

    I suppose next I need to try another computer.

    sphil.931Author
    Visitor II
    September 4, 2020

    How I solved this.

    The issue was the linux drivers from ST for USB and that specific version of ST-LINK failed to function correctly and or was broken. I am using Debian 10 (buster) 64 bit install, only a few installed applications from source so it was pretty much standard. When I more recently (June) went to use it I had the ST-LINK update utility etc. all updated and installed "the latest" drivers, update was still dysfunctional.

    Using a laptop running windows 10 and the windows USB driver that was installed for ST-Link worked without issue. So process of elimination, it's unlikely the JAVA app was different between systems so that only left the Run Time Environment, or the USB driver with that specific version of ST-LINK under linux.

    Anyhow it was fixed by bypassing update under linux.

    Hope this helps somebody :D

    Visitor II
    September 11, 2021

    How I partially solved this.

    I had the same problem on Linux (Cube IDE 1.7.0 on Ubuntu 20.04) and switching to Windows 10 did not solve it.

    What I dit was to go back to CubeIDE 1.1.0 on Linux and to do incremental firmware upgrades from that version (going through: 1.1.0 -> 1.3.0->1.4.0->1.6.1).

    The only upgrade that did not work was on 1.7.0.