ST-Link Utility CLI for STM32L151
Environment
Installed software:
STM32 ST-LINK utility (STSW-LINK004) v 4.4.0.0 ; (with its ST-LINK_CLI).
STM32CubeProgrammer (STM32CubeProg) v 2.0.0 (with its STM32_Programmer_CLI).
Hardware:
MCU: STM32L151CB.
Debugger: STLink/V2 hardware.
I am using ST-LINK utility to erase Data EEPROM of the MCU, as CubeProg can't do this over Command prompt (STM32_Programmer_CLI). (I am automating programming. So need to use CLI). And ST-LINK_CLI fails to disable RDP byte, before I need to upgrade the MCU firmware. So I need to use STM32_Programmer_CLI.
ST-LINK_CLI with "-Log" option does not store the log though it says so !
"Trace.log generated in the following folder :
C:\Users\<my_windows_user_ID>" where the log is not found though !
As per the document it should have been in C:\Users\<my_windows_user_ID>\STMicroelectronics\ST-LINK Utility\ . Log is not found here too !
My Q's:
ST-LINK_CLI doe not work well for Option Bytes section of this MCU AND, STM32_Programmer_CLI not enabled to erase the Data EEPROM.
Log is not working in ST-LINK_CLI.
Thanks !