ST/LINK-V/2 STM32H723ZGT6 program 1st time
Trying to connect to a STM32H723ZGT6 for the first time.
Does the ST/LINK-V/2 have to use the JTAG connection on this device as I feel it probably does?
The 4 pin connection being for the STM8 only?
I jave connected as a JTAG connection using jumper leads from the programmer onto the board.
*******************************************************************************************************
19:35:36 : UR connection mode is defined with the HWrst reset mode
19:35:36 : ST-LINK SN : 52FF6B064849825028390367
19:35:36 : ST-LINK FW : V2J43S7
19:35:36 : Board : --
19:35:36 : Voltage : 3.50V
19:35:36 : ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
19:35:36 : ST-LINK SN : 52FF6B064849825028390367
19:35:36 : ST-LINK FW : V2J43S7
19:35:36 : Board : --
19:35:36 : Voltage : 3.50V
19:35:36 : Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
****************************************************************************************************
I have checked the VDD caps all bypassed 100nF, VCAP bypassed caps 2.2uF and all seems good. Not sure what voltage I would see on the VCAP pins. I can see from the list I have the board powered at 3.5V. Not sure on what BOOT0 pin should be so it has been pulled low and high. VBAT is pulled high and bypassed with 100nF cap. Power supply looks stable. VDDA and VSSA connected to VDD and VSS respectively and bypassed with a 100nF. VREF+ strapped to VDDA using a 10K resistor.
I will shorten the JTAG jumper leads next butI do not think this is the issue... I just seem to be missing something.
I am attempting to detect the device using the CubeProgrammer or using a previous basic project in the CubeIDE.
Any suggestions on what may be the issue would be much appreciated.
Thank You.