Skip to main content
Visitor II
April 8, 2022
Solved

ST-LINK V2 Clone cannot upgrade firmware, so cannot proceed with STM32CubeIDE 1.9.0

  • April 8, 2022
  • 7 replies
  • 26852 views

Here is a sequence of screen captures demonstrating the problem I'm encountering (in particular, the firmware version displayed by the software appears to become same as the firmware version intended for upgrade; the upgrade says it failed, but then appears to complete, but does not actually solve the operational issue (subsequent attempt to use the device yields the following message in the console:)

"Error in initializing ST-LINK device.

Reason: ST-LINK firmware upgrade required. Please upgrade the ST-LINK firmware using the upgrade tool."

0693W00000LxQEzQAN.png0693W00000LxQEuQAN.png0693W00000LxQEaQAN.png0693W00000LxQEVQA3.png

    This topic has been closed for replies.
    Best answer by KnarfB

    A clone is only a clone, use at your own risk.

    hth

    KnarfB

    7 replies

    KnarfBAnswer
    Super User
    April 8, 2022

    A clone is only a clone, use at your own risk.

    hth

    KnarfB

    wb0gazAuthor
    Visitor II
    April 9, 2022

    Yes, just no experience with this device before --- turns out STM32 Programmer software (current version) supports the clone for programming/reading/etc., but no debugging, which is sufficient for the current need.

    Tks

    Explorer
    April 3, 2024

    now STM32 supports the clone stlinkV2 for debugging.

    thanks

    Visitor II
    April 9, 2022

    Just open your ST LINK V2 and see which ic inside other from ST is clone devices.​

    Visitor II
    June 18, 2022

    Clone is equipped with CKS 32F103C8, seems to be a non accurate alternative to STM32F103C8.

    wb0gazAuthor
    Visitor II
    June 18, 2022

    Agreed - I did find that type of device inside the clone unit; I now use STM32CubeProgrammer with this device as it is (at least in current version) accepting the clone unit's existing firmware; I use a genuine STLink device when necessary to use STM32CubeIDE 1.9.0 which will not accept nor upgrade the clone unit's existing firmware.

    Visitor II
    March 10, 2023

    i use

    STSW-LINK007 ver 2.36 so my st link updated to v 2.36

    then use STM32 ST-LINK Utility  in stlink menu update stlink to 3.37

    Visitor II
    November 11, 2023

    ya lo intente pero no me deja 

    st-link device lost when exiting update mode

     

    Visitor II
    November 11, 2023

    Alguien que tenga la solucion, ya se desde los archivos, porque desde el upgrate no me deja