Question
ST-LINK/V2 Commandline - HALT does't work
Posted on April 19, 2013 at 18:11
Hi,
for an automatic test, i need to Halt and Run a STM32. It works without problems with the STM32 ST-LINK Utility, but not (program is still running) when I use the CLI (st-link_cli.exe) in this way:st-link_cli.exe -c SWD -Halt the answer for this statement is:STM32 ST-LINK CLI v1.5.1
STM32 ST-LINK Command Line Interface
Connected via SWD.
Connexion mode : Normal.
ST-LINK Firmware version : V2J17S4
Device ID:0x416
Device family :STM32L1xx medium density All other statements give a message that the statment were accepted Can anyone check this, maybe with older firmware? What tool can I use alternativly? Thanks in advance Wolfgang #st-link #halt #st-link #cli