Question
ST-LINK V2 does not connect to STM32F103
Posted on March 31, 2015 at 13:21
Hello!
I have strange error while attempting to connect ST-LIK Utility to MCU. Trace log: W at 0xe000edf0: 0xa05f0000 cErrLog::SetLogTraceOn STLinkUSBDriver.dll loaded ST-Link/V2 device detected Target voltage detected: 1.557480 Driving NRST low W at 0xe000edf0: 0xa05f0003 R at 0xe000edf0: 0x02010001 R at 0xe000edf0: 0x02010001 Target is held under reset Activating vector catch system W at 0xe000edfc: 0x00000001 R at 0xe000edf0: 0x02010001 R at 0xe000edf0: 0x02010001 Driving NRST high R at 0xe000edf0: 0x02030003 R at 0xe000edf0: 0x00030003 W regId 16: 0x01000000 W at 0xe000edfc: 0x00000000 R at 0xe000ed00: 0x00000031 R at 0xe0042000: 0x00000014 R at 0xe0042000: 0x00000014 R at 0x1ffff7e0: 0x00000000 R at 0xe0042008: 0x00000000 W at 0xe0042008: 0x00001800 R at 0xe000ed00: 0x00000031 R at 0xe0042000: 0x00000014 R at 0xe0042000: 0x00000014 R at 0x1ffff7e0: 0x00000000 R at 0xe000edf0: 0x00030003 R at 0xe000edf0: 0x00030003 Error (0x17) after target cmd F2 3E 00 00 00 00 00 00 00 00 Error (19) in ReadMemory_32Bit (768 bytes from 0x8000000) Error (0x12) after target cmd F2 36 F0 ED 00 E0 00 00 00 00 W at 0xe000edf0: 0xa05f0000 Error (0x12) after target cmd F2 35 F0 ED 00 E0 00 00 5F A0 Error repeats on several MCUs. Firmvare version of ST-LNK V2.J23.S4. This debugger works with STM8 correctly.In what could be
problem?
#st-lik-utility