ST Link V2 doesn't connect the target after 1~3 times firmware download.(STM32G071R8T6)
Hi.
I want to use ST32G071R8T6 on my project.
As a first step, I was testing my firmware on NUCLOE-G071RB (that connected indivisual st-link board).
I was no problems and working well.
However, on the board I made, it behaves abnormally.
ST Link V2 doesn't forget the target after 1~3 times firmware download.
Has anyone ever experienced these symptoms or knows how to fix them?
I changed boot0 pin to pull-up, but the ST Link V2 didn't connect to target also.
Please give me an idea.
Thanks.