Skip to main content
Visitor II
January 13, 2017
Question

ST-Link/V2 no connecing but with JLinkPro no problem

  • January 13, 2017
  • 1 reply
  • 1678 views
Posted on January 13, 2017 at 12:49

Hi,

I have a problem with the ST-Link / V2. I have designed my own board and if I want to access the STM32L476RG via JTAG, the ST-Link Utility write the following lines into the Trace.txt file:

ST-Link/V2 device detected

Target voltage detected: 3.508662

Error (0x8) after target cmd F2 30 A4 00 00 00 00 00 00 00

Error (19) while initializing ST-Link in JTAG mode

If I use a Segger JLink Pro, I can flash and debug the MCU without any problems.

Can anyone explain this?

best regards

Roger

#jlink #st-link/v2

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.

    1 reply

    Visitor II
    January 13, 2017
    Posted on January 13, 2017 at 14:40

    Hi

    Heil.R

    ‌,

    Could you please precise the ST-LINK and the ST-LINK Utility

    version are you using?

    Is this behavior observed also when

    connecting via SWD?

    -Nesrine-

    Visitor II
    January 16, 2017
    Posted on January 16, 2017 at 08:56

    The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6rG&d=%2Fa%2F0X0000000bwp%2FJ9ZkO3jCBCf8y5gvVBmC7yf1LRBOTmGhKNsCSQo_SWY&asPdf=false
    Visitor II
    January 16, 2017
    Posted on January 16, 2017 at 10:12

    Hi

    Heil.R

    ‌,

    Try to upgrade firmware version:

    STM32 ST-Link Utility>ST-Link>Firmware update

    -Nesrine-