ST-LINK/V2 unable to program a custom board with STM32F446RCT7TR
Hello people,
The problem:
Is my first time working with a custom board and I have:
- ST-LINK/V2 programmer
- JTAG 20 PIN 0.1" TO 10 PIN 0.05" ADAPTER
- Custom board with an STM32F446RCT7TR
I use the adapter to connect the ST-LINK/V2 to the programming port in the custom board.
What I do:
- Connect the ST-LINK/V2 to the board
- Connect the ST-LINK/V2 to the PC
- Power on the custom board
- Go to the STM32CubeProgrammer
- Finally connect to the board
All I get is an error: No STM32 target found.
Attached is the configuration I'm using (I tried almost all of them)
12:47:06 : ST-LINK SN : 36FF6A064246363828481057
12:47:06 : ST-LINK FW : V2J37S7
12:47:06 : Voltage : 0.74V
12:47:06 : Error: No STM32 target found!
12:47:09 : ST-LINK SN : 36FF6A064246363828481057
12:47:09 : ST-LINK FW : V2J37S7
12:47:09 : Voltage : 0.83V
12:47:09 : Error: No STM32 target found!
12:47:13 : ST-LINK SN : 36FF6A064246363828481057
12:47:13 : ST-LINK FW : V2J37S7
12:47:13 : Voltage : 0.83V
12:47:13 : Error: No STM32 target found!I had the feelling that the problem was my ST-LINK, but I used to test other STM32 development boards that I have (which do not have a port like the ST-LINK or the adapter) and it works perfectly if I connect the cables in SWD mode
VCC
SWDIO
SWCLK
GND
Do you know what exactly is the issue? I already ordered another ST-LINK/V2 to see if this could solve the issue.
I tested just only the 3v3 volts in the programming port from the custom board and it looks ok (it gives 3v3 for the programmer) so I am open to suggestions.
Thanks!!