Skip to main content
Visitor II
April 15, 2015
Question

ST-LINK/V2 under Windows 2000

  • April 15, 2015
  • 1 reply
  • 678 views
Posted on April 15, 2015 at 21:14

Hello, I need to program an STM8AF5289TC using an ICT Tester / Fixture and I just saw that ST-LINK/V2 Works just fine and is small and not expensive for integration, but the problem is that PC controller is Windows 2K, I have been looking thru the ST site and only XP,Vista, 7 and 8 drivers are available. Does anyone know if this programmer could work on W2K? are drivers available for it?

Thanks

#st-link-driver-w2k
    This topic has been closed for replies.

    1 reply

    Graduate II
    April 16, 2015
    Posted on April 16, 2015 at 18:13

    At this point no one is going to write specific support drivers for W2K, so either the available ones work, or not. Try downloading and installing the driver and ST-LINK utilities and see if they work. Try it on a DISCO board if you have one, about $10 if you don't want to spring for a ST-LINK/V2