Skip to main content
Visitor II
December 6, 2022
Question

st link v2 version v2j40s0 support stm32g0b0ret6 controller...???

  • December 6, 2022
  • 3 replies
  • 1429 views

hello everyone 

I am new to this stm32 series i purchased the stm32g0b0ret6 controller and now i am using stlink version v2j40s0 but i am getting the error no target device found can anybody guide me for that 

    This topic has been closed for replies.

    3 replies

    Visitor II
    December 6, 2022

    no idea Bro i am also searching the same .

    Graduate II
    December 6, 2022

    https://community.st.com/s/question/0D53W00001yz10FSAQ/does-stm32g0b0-controller-support-st-link-v2-debugger-or-not

    Vague anecdotal reports are hard to diagnose.. lead with as much detail as possible.

    Super User
    December 6, 2022

    Genuine ST-Link or cheapie/chinese clone?

    A custom board or NUCLEO, etc. eval board?

    Are you using the STLink utility or the STM32CubeProgrammer? You may need to use CubeProgrammer as the STLink utility is not being updated and most likely doesn't support G0 CPUs.

    If a custom board check your power supplies and all the various VDD pins (even the VDDA if the G0 has one). Is the reset pin connected to your debug connector?

    prasad1Author
    Visitor II
    December 7, 2022

    0693W00000WKPWeQAP.jpgi have this connection to stlink v2 clone and i am using stm32cube ide

    pins connection to st link v2 are

    VCC - 19 of stlink v2

    VSS/GND - 20

    swdio- 7

    swclk - 9

    prasad1Author
    Visitor II
    December 7, 2022

    Hi, found the solution.. reset circuit must be connected and program is done using STM CUBE IDE.

    we can program G series with st link v2 .