Question
ST-LINK V2 Virtual Machine speed
Posted on February 05, 2013 at 07:05
Hi All,
I am using Keil uVision 4 with the ST-Link in the STM32L Discovery board. I can load a 150K binary on my windows machine in less than a minute but on my virtual machine it takes close to 4 minutes! The virtual machine is running on a macbook pro with beefy specs [ 2GHz Quad i7 with 12GB RAM , 4Gb for the VM and a SSD hard drive ] . I know the specs dont matter as much for the transfer speed but I cannot figure out why the performance would be so different. I am flashing using SWD [ not JTAG ] not sure if that makes a diff either. Any help here is appreciated! Thanks #st-link #stm32-discovery