ST-Link v3 Mini with STM32CubeIDE
Hi
I am using STM32CUBEIDE on macOS. Until now I used my ST-Link v2 via SWD with no problems. I have recently upgraded to an ST-Link v3 MINI and implemented the STDC14 connector on my custom pcbs. The pinout is according to the datasheet (the pins on the ST-Link are numbered and DIO is 4, CLK 6 and so on..)
however: when I open STM32CUBEIDE it recognizes the st-link but when I hit run or debug, it will return "no target found". When I disconnect the ST-Link v3 and connect my st-link v2 I am able to flash the board with no problems.
the ST-Link v3 MINI led is always red during this process.
Does anybody have a clue on how to handle this? I also did not manage to use the drag&drop function...