Skip to main content
Explorer
December 1, 2025
Question

ST‑LINK V3 Minie connects to STM32F100RBT6B Discovery but not to my custom board

  • December 1, 2025
  • 2 replies
  • 194 views

I’m using an ST‑LINK V3 Minie with an STM32F100RBT6B Discovery board (which also has an STM32F103C8T6), and it works perfectly. However, when I connect the same ST‑LINK V3 Minie to my custom board that uses the same STM32F100RBT6B chip, it fails to connect.

I’ve wired VCC (VTref), GND, NRST, TMS/SWDIO, and TCK/SWCLK exactly as specified.

Black - Ground

White - Vcc

Yellow - Reset

Blue - Clock

Purple - TMS

On the Discovery board this setup works fine, but on my custom board the debugger cannot establish communication.

Could anyone suggest what additional checks I should perform on the custom board?

 

 

    This topic has been closed for replies.

    2 replies

    Explorer
    December 1, 2025

    Doesn't this suggest the problem is with your custom board ?

    I would suggest to connect the VDD /T_Vcc pin as well, as it is used to sense of the target is powered :

    Ozone_0-1764569768155.png

    Have you checked the voltage at the supply pins of you custom board (at the MCU pins), and the power consumption ?
    Only then would I connect an external tool like a debug adapter.

    saranAuthor
    Explorer
    December 1, 2025

    @Ozone Yes I have checked the voltage supply at Vcc, it gives 3.3V.

     

    Explorer
    December 1, 2025

    I don't know if you understand what I meant.

    First, make sure your PCB is correct.
    Check all traces for the MCU's power supply, debug connection, clock generation etc., preferably unpowered first.
    Then apply power (if possible with a current limitation enables), and measure current draw.
    Only then connect to a debug adapter.

    AFAIK the ST-Link adapters don't require a T_Vcc detection. I converted basically all my ST-Links into J-Links.
    If you don't get connection, try a scope (or logic analyser) and check the debug signals.

    Alternatively you can try to start the MCU into system mode (via BOOT0), and try connecting via serial line & CubeProgrammer.
    I suppose you planned for an option to pull BOOT0 low for this purpose.

    Super User
    December 1, 2025

    Where are your bulk and decoupling capacitors? They should be next to the chip.

    Could also be cold solder joints and/or bridges. Hard to tell in the photo.

    TDK_0-1764599964429.png

     

    Marking on the top left of the chip looks like the mold injection mark, not the pin 1 marking, but I don't see a pin 1 marking elsewhere, or any text marking on the chip. Ensure orientation is correct. Pin 1 is bottom left when text reads from left to right.

    TDK_1-1764600150089.png

     

    saranAuthor
    Explorer
    December 2, 2025

    @TDK @Ozone Thanks for your inputs. But the custom board works well with STlink - V2 debugger and programmer.

    Super User
    December 2, 2025

    Probably the wiring is incorrect, then.

    Does STM32CubeProgrammer report the correct voltage?

     

    Use a standard debugging header to avoid all of this.