Question
ST-Linkv2 on STM32F3 Discovery
Posted on June 08, 2015 at 16:33
Hello,
I've been using STM32 for quite some time. In work I use full ST-Link v2 isol but, in home as hobbys (and soon startuper) I use stlink on stm32f4 disovery board. I had no problems with it untill today. When my external board is fully powered by Disco. (is connected to 3V and GND) everything works. I can flash it, erase etc. However when I connect external power supply to external board (which is 3V45) I cannot connect to device. With STM32 utility I get ''Can not connect to target'' but still I get Device ID, and type but cannot flash it or read memory. Questions are:1) Is it normal?2) If I get full ST Link v2 (not isol) will it help? #stm32f4 #discovery #stlink