STlink debugging hardcoded to start at Reset_Handler address ignoring vector table values.
STM32F030R8
Blank project, no CMSIS, no Cube libraries.
Code copied from my old TrueStudio project.
I use old startup_stm32f030x8.s with some modifications.
If I change startup vector table start entry to my function (named not Reset_Handler but Boot_Start), then
compiler works OK,
elf contains correct vector table
downloads and runs OK
BUT
debugging by ST-Link (with unchecked "Resume" in Startup Debug Configuration settings):
debugger shows my function (OK)
disassembler window shows my function (OK)
BUT
PC register is set to Reset_Handler address (or junk if no such symbol)
and attempt to step or run will go to bad address.
Well,
I can rename my startup function into Reset_Handler and old Reset_Handler (I will jump there in the end) in some Old_Reset_Handler. Then I can debug my bootloader and my application.
Nevertheless it's an IDE Bug.
(TrueStudio performed OK in that case).