STLink firmware bug regression: Target does not boot when powered by E5V
From finds on the web, there was, years ago, the phenomenon with STM32 Nucleo boards that, when J5 is set to E5V, and the board is powered from the E5V pin instead of USB, the target MCU will be held in reset.
I just updated the ST-link firmware on a nucleo F103RB board with the firmware that is offered by CubeIDE 1.6.1.
The firmware version was something with "3.J7..."
I then observed this effect.
My installed ST-Link Util software offered a lower version, 3.J4 something.
I downgraded to that - now it works again, i.e. the target MCU runs when externally powered and nothing is connected to the debugger USB jack.