STLINK Problem , (possibly p-nucleo bricked ?)
Hi
This is the first time I`m using STM32 tools and probably made a mistake hence I can`t connect to Nucleo 68 board.
When I try to connect using STLink Utility I receive
22:31:40 : Can not connect to target!
Please select "Connect Under Reset" mode from Target->Settings menu and try again.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
22:31:41 : No target connected
On the settings it shows as - Target detection fail. / Target Voltage Detection fail
When I connect it for the first time I was able to debug using Keil but debugger crashed in a function and next I tried to Load the program . This is where board became unresponsive
Has anyone experienced something similar this ? How do you unbrick a board ?
Thanks