Skip to main content
Visitor II
May 17, 2015
Question

STLink V2 not detect on Dell Notebook

  • May 17, 2015
  • 2 replies
  • 586 views
Posted on May 17, 2015 at 12:48

Hi,

I have a STM32F4-Discovery and the ST-Link V2 is not detect on my Dell Latitude 3540, I tried all usb ports, when I plug the usb connector windows not detect nothing. I tried on another PC and is working without problems. On my notebook many another usb periphericals is working without problem.

Suggestions?

Thank you

Giovanni

#stlink
    This topic has been closed for replies.

    2 replies

    Graduate II
    May 17, 2015
    Posted on May 17, 2015 at 16:11

    Different versions of Windows? Which?

    Different USB ports? All?

    Shows up in Device Manager? Or Not?

    juvannAuthor
    Visitor II
    May 20, 2015
    Posted on May 20, 2015 at 13:44

    The problem is not OS I tried Windows 7 and Linux.

    My notebook has 4 USB ports: 2 USB3.0 and 2USB2.0 and in all ports there is the problem, I tried also with HUB.

    In linux in dmesg not appear nothing also errors, in Windows nothing in Device Manager and I don't receive also the sound notification, it's invisible.

    I

    f

    it did not work

    on another PC

    I would have said

    is broken.

    I tried 5 USB cables without success.

    Thank you

    Giovanni