Question
STLINK-V3 Mini UART doesn work from the edge connector
Hi EveryOne!
I use a brand new ST-Link V3 Mini shield and would like to use its Virtual Com-Port feature with connection via its Edge connector. SWD works well but UART doesn't at all.
I use pin 1 & pin 11 for connection to UART but no result.
PS. If I use the same shield but use STDC14 connector cable and its 13&14 pins then UART works via these pins. What can be wrong with 1 & 11?