Skip to main content
Graduate
April 30, 2020
Question

STLINK-V3MINI / MODS Schematic

  • April 30, 2020
  • 6 replies
  • 5840 views

Hello, I would like to integrate ​STLINK-V3MODS into my own board, but I can't find the internal schematic of STLINK-V3MINI or MODS anywhere.

Is it possible to obtain MB1467 schematic?

Thanks

    This topic has been closed for replies.

    6 replies

    Visitor II
    March 18, 2021

    Anyone at ST going to answer?

    Graduate II
    March 19, 2021
    Visitor II
    March 19, 2021

    If only, CN3 has no voltage on the MOD, it is missing parts and CN5 pin one can't have 3V3 and PB0 on pin 1, if PB0 was pulled low there would be problems. The only way I can handle this issue is a BUCK/BOOST regulator from external Vref taking 1.8V or 3.3V or 5V to 5V with a 3.3V LDO for the MOD IO. and three LSF0108 voltage translators giving me I2C, SPI, GPIO, CAN, UART, JTAG at 1.8V~5V external programming. I added a CAN transceiver which needs 5V on the differential side. The shield would be 40X34mm 15mm high. I don't understand why they don't publish the MOD/MINI device information.

    Visitor II
    March 28, 2021

    Hi,

    can ST guys publish info about missing parts on MODS ? So i can soldering myself and use as MINI.

    Thanks

    Visitor II
    May 27, 2021

    Bump?? I also want to know the difference between V3 MODS and MINI

    Graduate II
    May 27, 2021

    I could swear there was another thread on this, but yes Schematics and Mechanicals really shouldn't be too big an ask...

    There was one on the V3SET sub-boards yesterday as well.

    @STOne-32​ 

    Graduate II
    May 27, 2021