STLINK-V3MODS Edge Connector Pin 30
Hi, there
I'm trying to integrate the STLINK-V3MODS with my STM32H745 based project.
The STM32H745 MCU is powered by an external 3V3 output regulator.
The STLINK-V3MODS board has the following edge pin:

Which is described in the manual as an "Input for STLINK-V3MODS". Now, I'd like to know if I should tie this pin to my 3V3 board voltage, for the MODS to function correctly. Or, if I can just leave this pin floating.
The only functionality I need from the MODS board is to 1. Debug the H745 MCU; 2. Carry serial data via the UART line.
I know that the MODS board powers via USB, hence why I'm a bit confused about this pin 30.
Thank You!