STLINK-V3MODS for custom PCB
Hi Community,
I'm designing a custom H755 board and had intended to implement my own USB-C with debug/programming interface using an external STLINK module.
STLINK-V3MODS is a nice alternative way forward but I note from the user manual (UM2502) that it can only deliver up to 200 mA at 5V, whereas I need around 500 mA.
Is there an alternative debugger-progammer module that I can use, whilst also using this to deliver 5V with enough power to supply my board (power taken from USB obviously)?
I want the option to use a power-bank battery pack to power my circuit in normal operation, but the ability to program and debug via USB.
Thanks