STLINK-V3PWR Connection to legacy targets
How does one connect the STLink debug port to an older target with 0.025 square posts on 2.54 mm ptch for the debug connections? As best I can tell, the supplied cables only support 1.27 mm pitch,
How does one connect the STLink debug port to an older target with 0.025 square posts on 2.54 mm ptch for the debug connections? As best I can tell, the supplied cables only support 1.27 mm pitch,
I finally got around to using my STLINK-V3PWR or trying. The issue is lack of thought on STM side, one simple adapter like all those ARM adapters but with a 10 pin 1.27mm pitch connector instead of the 2.0mm pitch they have. I purchased the V3PWR since it has a type C connector instead of the micro USB connector and all the power stuff my standalone power board does but with a case. I think I'll have to make a cable, after hunting for several hours I see no solutions. I had one of these https://bit.ly/4g6lPst laying around, with some soldering and crimping it's a start. A real solution would be a bundle like this https://bit.ly/3D9dA0l with a 1.27mm pitch 10 pin instead of the 2mm pitch 10 pin connector.
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.