STLINK-V3PWR not supported by STM32CubeIDE V1.1.12
I'm running on Mac-OS with CubeIDE V1.12.1 (the latest at this time)
When I try to connect a target using SWD with my STLINK-V3PWR probe I get the following:
"No ST-Link detected" in a popup named : "ST-LINK firmware verification"
If I try to upgrade the probe firmware from the IDE menu 'Help"->'STLINK upgrade' , this lead to a downgrade from V4J2B1P4 to V4J1B1P3 (the STLinkUpgrade tool has Version 3.11.3 , not the latest one 3.12.3)
I tried to downgrade the probe firmware with no success with target connection.
The CubeMonitor-Power application works (but I have the same, already reported in forum) problem of OVC triggering on power-ON on VOUT due to inrush current to the target
I tried also STM32CubeProgrammer that connects to my target with SWD, so the probe is properly connected to the target ... by the way, the StLinkUpgrade.jar included in the last STM32CubeProgrammer application is an old one not even recognising the STLINK-V3PWR !!
I suppose I have to wait for an CubeIDE release to have this probe working ?