Skip to main content
Visitor II
December 12, 2025
Question

STLINK v3SET not recognized by PC

  • December 12, 2025
  • 1 reply
  • 53 views

Hi, just bought a STLINK-V3SET to use with EVSPIN32G02Q1S1 evaluation board.

It doesn't seem to be able to connect via USB. I've previously recently used STLINK v2ISOL and it worked as expected, so i already had the driver installed and it should be the same driver.

Tried different cables, different PCs, different USB ports, reinstalling the driver: to no avail.

So what can be the reason here? I'd appreciate any suggestions.

    This topic has been closed for replies.

    1 reply

    Visitor II
    December 12, 2025

    Some additional info:

    when i connect the device to the computer, there is no reaction.

    No "device connected" sound, no new devices in the device manager.

    The LEDs are both on; the red one (COM) is blinking and the green one is continiously one (PWR).